Back to Main Menu

Service Index

Objective: Gain an understanding of what a Service Index is, and how to configure it in Predictor. 

Predictor’s Service Indices function is typically utilized for reporting purposes where models have more than one Service Criteria identified and configured for each of the assets. Predictor templates begin with one default Service Index, named OSI (Overall Service Index), which always uses the Weighted Average calculation method and is typically configured to utilize all of the Service Criteria multiplied by their Allocated Weightings to calculate and return a condition state for all assets on an individual basis, which provides an overall condition number and can be used as the default reporting index.

 

However, when the models configured utilize service condition drivers for different elements or components of the asset, the OSI calculated based on these values can be skewed, as it utilizes all service condition criteria to calculate the final condition state. This may be acceptable for certain models, however, this is not always the case. Consider the following example:

 

A buildings model has been configured that utilizes Roof Cladding condition, Substructure condition, Superstructure condition and External Wall Surface Finish condition. Whilst the External Wall Surface Finish condition criteria is required to drive the model with regards to painting or rendering works, this service criteria will not play a major factor in the calculation of the building asset’s structural state.

 

If the condition state for the External Wall Surface Finish was 5, or poor condition, but all conditions were rated as 1 or 2, the Overall Service Index could be equal to 3. This would mean that an aesthetic criteria was inflating the final Overall Service Index.

 

However, if we were to exclude External Wall Surface Finish condition, the calculated condition is more reflective of the structural components of the building asset. In a case such as this, it would be recommended to use and configure the Service Index to more accurately report the condition of the various asset elements and components as applicable, thus improving the OSI. Alternatively, an additional Service Index could be added and configured differently from the OSI.

 

Note that the Service Indices can only be set up if Service Criteria were created in the Template, as they are a variable that controls the importance and weighting attributed to a set of Service Criteria.

 

To configure the Service Index:

  • Click the Service Index tab within a Template
  • Click the Add button in the Service Indices box:

Users can edit and remove service indices using the Edit and Remove buttons.


The following screen will appear after Add is clicked:

 

Using the arrow buttons, users can select the services that would come under each service index. In the above screen, the User has created a service index called Structure Disruption and selected three services that describe the physical condition of the asset under that service index.

It is also possible to select the method by which the Service Index is calculated. The different methods are as follows:

 

Weighted Average Multiplies the nominated service criteria by the assigned weightings which are then divided by the sum of the weightings.
Worst Value Returns the highest value of each of the nominated service criteria.
Average Value Assigns a straight average of all nominated service criteria without the need to apply weightings.
Best Value Returns the lowest value of each of the nominated service criteria.
Weighted Worst User Defined Selects the highest value of the nominated service criteria and then adds the sum percentage of each of the remaining scores to that value.
Custom Formula Allows users to build a custom calculation logic for the Service Index.

 

Selecting Custom Formula will open the Expression Editor. Using this, users can add fields, operators, and functions, in order to define the custom logic for the Service Index.

 

The Expression Editor allows for any of the Service Criteria in the Template to be added as fields to the expression, and combined with arithmetic operators (addition, subtraction, multiplication, division) and functions (maximum, minimum, average, total), in order to define exactly how the resulting Service Index will be calculated.

 

Once the Custom Formula has been configured, it will also be visible in the Transformed Data. Note that the fields used in the Custom Formula may rely on the configured Data Mapping.